Browse FAQs

Modular PDU Breaker LED Light Staying Green or Not Changing State

Published date: 06 September 2016

 

Issue:
Modular PDU Breaker LED Light Staying Green or Not Changing State
 
Product line:
Modular PDU
 
Environment:
Opening and closing of breaker does not change the LED status light on breaker
 
Cause:
If the Modular PDU Alarm Status if set to Off, the breaker will never change state. So the Green LED will always be lit
->
If the Modular PDU "Alarm Status" and "Position Alarm" is set to Off, the breaker will never change state. So the Green LED will always be lit

Resolution:
            In the Web interface of the PDPM, within the settings of each module, the “enable” box needs to be checked so the alarm and LED will trigger.
The “Mass Configuration” option is available only when looking at the “all locations” screen.
->
            In the Web interface of the PDPM, within the settings of each module, both “enable” box needs to be checked so the alarm and LED will trigger.
The “Mass Configuration” option is available only when looking at the “all locations” screen.
 


 





Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.