Browse FAQs

Video: How configure the Display and Beeper on an InRow ACRD200 cooling system

Published date: 27 April 2018

Issue:
How configure the Display and Audible options on an ACRD200 cooling unit

Product line:
ACRD200

Environment:
All Serial Numbers

Cause:
Install, Configuration

Resolution:



Press ESC until you get to the main screen (On/Standby)
 
Use the Up or Down arrows to find the heading Configure Display
 
Press ENTER and select Contrast
 
Now you will be prompted for a password
 
Use the default password of “apc”
 
If this does not work check with your Admin for the correct password
 
If password has been lost use the last eight digits of the serial number
 
Press Enter and set Contrast from 1-10. This changes the brightness of the screen.
 
Press Enter on Key Click and turn On or Off. This allows every key on the display to make noise when used.
 
Press Enter on Beeper Volume you can select Low, Medium, or High. This controls the level of the Beeper volume in turned on.
 
Press Enter on Beep On Alarms and select ether On or Off. This enables the unit display to beep if unit is in alarm.
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.