Browse FAQs

Power Over Ethernet configuration supported by NetBotz products.

Published date: 13 November 2013

Issue:

Power Over Ethernet configuration supported by NetBotz products

Product Line:

NetBotz

Environment:

NetBotz version 3 Rack appliances and POE

Cause:

POE options that work with supported NetBotz version 3 rack appliances.

Resolution:

IEEE compliance offers 2 alternatives for Power Over Ethernet (POE). Alternative 'A' allows for power to be passed through wires 1, 2, 3, and 6 on a Cat-5 switch are the transmit and receive wires. Alternative 'B' allows for power to be passed using the unused pairs 4, 5, 7, and 8 on a Cat-5 cable.

Alternative 'A' is usually output by a switch or endspan device. Alternative 'B' is more often used by a midspan device such as a POE injector. APC's POE injector (NBAC0303) inserts power on the Cat-5 cable using alternative 'B'

NetBotz POE compatible appliances work with either alternative and should power on with alternative 'A' or 'B'.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.