Browse FAQs

Serial devices on a Netbots connected to the same port as a camera pod can cause bot to reboot.

Published date: 14 August 2013

Issue:

Serial devices on a Netbots connected to the same port as a camera pod can cause bot to reboot.

Product Line:

NetBotz

Environment:

All versions

Cause:

RS232-based Serial Devices connected to a USB-to-Serial Port adapter and USB modems should not share the same USB port or hub as a Camera Pod 120, Camera Pod 160, or a CCTV Pod 120. Doing so may cause configured USB-based Serial devices to disappear and then reappear, or your appliance may unexpectedly restart

Resolution:

Make sure these devices use different ports or hubs.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.