Browse FAQs

Details Returned from Compaq Devices via Advanced Device Crawlers

Published date: 10 May 2018

Issue:

Details Returned from Compaq Devices via Advanced Device Crawler

Product Line:

NetBotz

Environment:

NetBotz version 2 Advanced Device Crawlers.

Cause:

The following information can be queried via Advanced Device Crawlers for Compaq systems assuming the Compaq DDF (Device Definition File) is installed on the NetBotz appliance and the Compaq system is SNMP enabled. Please note that not all information listed below is available on all Compaq models.

Resolution:

 
  • Description
  • Overall Thermal Condition
  • Thermal Degraded Action
  • Temperature Status
  • Fan Status
  • CPU Fan Status
  • Fan Present
  • Fan Type
  • Fan Speed
  • Fan Redundancy
  • Fan Condition
  • Power Supply Present
  • Power Supply Condition
  • Power Supply Status
  • Power Supply Main Voltage
  • Power Supply Capacity Currently Used
  • Power Supply Maximum Capacity
  • Power Supply Redundancy State
  • Power Converter Module Present
  • Power Converter Module Slot
  • Power Converter Module Socket
  • Power Converter Module Redundant
  • Power Converter Redundant Module Group ID
  • Power Converter Module Condition
  • Storage System Box Type
  • Storage System Box Condition
  • Storage System Fan Status
  • Storage System Temperature Status
  • Storage System Side Panel Status
  • Storage System Fault Tolerant Power Supply Status
  • Storage System Box Placement
  • Storage System Connection Type
  • Storage System Chassis Overall Condition
  • Storage System Power Supply Condition
  • Storage System Fan Condition
  • Storage System Temperature Condition
  • Storage System Fibre Channel Array Controller Condition
  • Storage System Fibre Channel Array Logical Drive Condition
  • Storage System Fibre Channel Array Physical Drive Condition
  • Storage System Backplane Condition
  • Storage System Power Supply Status
  • Storage system Power Supply UPS Status
  • Storage System Power Supply Condition
  • Storage System Fan Module Status
  • Storage system Fan Module Condition
  • Storage System Temperature Sensor Status
  • Storage System Temperature Sensor Condition
  • Storage System Temperature Sensor Value
  • Storage System Backplane Condition
  • Storage System Backplane Fan Status
  • Storage System Backplane Temperature Status
  • Storage System Backplane Fault Tolerant Power Supply Status
  • RAID Storage System Status
  • RAID Storage System Condition
  • UPS Line Status
  • UPS Name (type)
  • UPS Battery Time Remaining (minutes), (-1 = not supported)
  • UPS Alarm Text

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.