Browse FAQs

Details Returned from Cisco Devices via Advanced Device Crawlers

Published date: 26 May 2015

Issue:

Details Returned from Cisco Devices via Advanced Device Crawlers

Product Line:

NetBotz

Environment:

NetBotz version 2 Advanced Device Crawlers.

Cause:

The following information can be queried via Advanced Device Crawlers for Cisco systems assuming the Cisco DDF (Device Definition File) is installed on the NetBotz appliance and the Cisco device is SNMP enabled. Please note that not all information listed below is available on all Cisco models.

Resolution:

 
  • Advanced Details
  • Voltage Monitor
  • Temperature
  • Fan Status
  • Power Supply Status
  • Fan Status
  • Chassis Minor Alarm
  • Chassis Major Alarm
  • Temperature Alarm

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.