Browse FAQs

USB Power Usage Guidelines for Netbotz

Published date: 30 April 2015

Issue:

USB Power Usage Guidelines for Netbotz version 2

Product Line:

NetBotz

Environment:

NetBotz version 2

Cause:

Power usage for NetBotz version 2. In the explanation below, 1 "point" of power is equal to 100 mA.

Resolution:

NetBotz USB Device Power Consumption
  • The Sensor Pod 120 requires 1 point of power.
  • The CCTV Adapter Pod requires 1 point of power.
  • The Output Relay Pod requires 1 point of power.
  • Wireless Receiver 120 requires 1 point of power.
  • The Camera Pod 120 requires 4 points of power.
  • The 4-20mA Pod requires 5 points of power


Note: The 4-20mA Pod must be connected directly to the USB port on the appliance or directly connect to the USB port on a externally powered USB hub.

Guidelines
  • The USB ports on the NetBotz Unit provides 5 points of power each.
  • 5 points being the maximum amount of power available per USB port.
  • All USB ports on self powered hubs provide 5 points of power each.
  • A self power USB hub does not consume power from the USB bus.
  • A bus powered hub consumes 1 point of power then divides the remaining 4 points of power among its downstream devices. A typical 4 port bus powered USB hub would provide 1 point of power for each of its USB ports.
  • A USB repeater or extender consumes .1 point of power and passes all remaining power downstream via its single USB port. So using USB repeaters, four of these could be daisy-chained which would consume .4 points of power. This makes available 4.6 points of power at the end of the fourth USB repeater. Therefore, it is acceptable to place a Camera Pod 120 at the end of a daisy-chain of four USB repeaters.
  • Maximum USB distance including hubs, repeaters, and standard USB cables (excluding fiber and cat5 pod extenders) is limited to 80 feet.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.