Browse FAQs

Using the Male to Male BNC Adapter Included in a Day/Night CCTV Camera (NBAC0224)

Published date: 23 January 2014

Issue:

Using the Male to Male BNC Adapter Included in a Day/Night CCTV Camera (NBAC0224)

Product Line:

NetBotz

Environment:

NetBotz NBAC0224

Cause:

Physical configuration options.

Resolution:

The NetBotz Day/Night CCTV Camera has a BNC female output.

The NetBotz CCTV Pod has BNC connection that looks like a male connector but it actually has a hole in the male connection so it will accept the male-male adaptor included with a Day/Night CCTV Camera.



Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.