Browse FAQs

Camera Motion Detection and Video Capture Overview - Version 2 Appliances

Published date: 04 February 2014

Issue:

Camera Motion Detection and Video Capture Overview - Version 2 Appliances

Product Line:

NetBotz

Environment:

NetBotz version 2 and 3

Cause:

All NetBotz Version 2 Appliances (320/420/500) support camera motion detection. It works by constantly taking pictures and capturing the current picture with the previous picture in its buffer. When motion is detected, then pictures are captured according to the Alert Capture Configuration for the camera:

Resolution:


When a camera captures pictures as a result of an alert / threshold, remember the following:

* Pictures are captured for a finite amount of time
* Once the defined amount of video is captured, no more video is captured until the alert condition clears and then starts again.



Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.