Consultar las preguntas frecuentes



Hardwiring to 120v, 208v, and 240v loads from a 208v/240v SmartUPS RT UPS
6U ) ... will see 208 volts (or 240v ... not two balanced 120 volt legs as you ... ... down transformers, APC manufactures 4 larger ... ... To supply a 120 v load, the ... 2 120 volt legs that are ... ... 240 v/ 120 v panel where there ... 2 legs of 120 v and from hot ... would measure 240 volts . 120 v Hot Leg ... phase from the 120 v leg) ... would measure 208 volts from Hot to ... ... legs that are 120 degrees out of ... A split phase UPS will require a 4 wire input and will output 2 balanced 120 v legs, a ground, and a neutral.
Can a 3rd party UPS be installed in the ar106v or ar106vi?
Cause: The NetShelter WX 6U Vertical cabinets have a mounting bracket for a 2U UPS.
How do I update the firmware of my SRT, SMC, XU, XP, SMX, SMT, SMTL, SCL, SRC, CHS series Smart-UPS?
Devices that do *NOT* have upgradable firmware: These units are 120 V devices built prior to date code 1037. Date code is the first 4 numbers in your serial number.
How do I update the firmware of my SRT/SMC/XU/XP/SMX/SMT/SCL/SRC/CHS series Smart-UPS using the Firmware Upgrade Wizard?
Issue: These units are 120 V devices built prior to date code 1037. Date code is the first 4 numbers in your serial number.
Video: How do I configure a 208v Smart-UPS RT or SRT for use with a 240v input?
If you need 120 v for your equipment you will still need to use a stepdown transformer.
Are the new 6U, 9U and 12U NetShelter cabinets hinged in the rear, like ar100 & ar100hd?
Issue: Customers inquire if the newer 6U , 9U and 12U wall mount cabinets are hinged in the rear.
Does the NetShelter WX castor kit AR8359 fit onto the ar106, ar109 or AR112.
Issue: There doesn't appear to be a castor kit for the 6U , 9U or 12U NetShelter WX cabinets .


Resultados 1 - 10 de 21

¿No encuentras lo que buscas?

Ponte en contacto con nuestro equipo de atención al cliente para obtener información sobre asistencia técnica, asistencia para quejas, etc.