APC Network Management Card provides remote monitoring and control of an individual device such as a UPS or PDU by connecting it directly to the network with a traditional ethernet cable or wirelessly with the APC USB Wi-Fi device (on certain models).

Security Enhancements
APC Network Management Card has modified its security features to reflect the new internet connected device requirements.
Enhanced Security, What’s Changed?
Next Generation Features
What is the End-of-Life support of Network Management Card 2?
The 2nd generation network management card end of sales date is December 2020. There is an additional year of support for firmware updates to reflect any further security changes.
For more information regarding product support read the End-of-Life policy document.
How do I know which card is installed in my device?
Upon login, the top banner on the interface specifically states which card is installed. Smart-UPS with a bundled network management card packaging also explicitly calls out which card is present.