Issue:
NetBotz 755 manual incorrectly states 12 AP9520T/TH sensors supported
Product Line:
NetBotz
Environment:
NBWL0755
Cause:
An incorrect notation in the initial NetBotz 755 manual states that up to 12 AP9520T or AP9520TH A-link sensors are supported
Resolution:
The NetBotz MBWL0755 only supports up to 4 AP9520T or AP9520TH A-link sensors and the manual is incorrect. The manual will be changed but in the meantime, we've added this FAQ to hopefully limit confusion.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.