{"searchBar":{"inputPlaceholder":"Search by keyword or ask a question","searchBtn":"Search","error":"Please enter a keyword to search"}}
{}

Our Brands

{"support":{"yesButton":"yes","noButton":"no","feedback":{"title":"What can we do to improve?"},"submitButton":"Submit","successMessage":"Thank you for your feedback","title":"Was this helpful?","feedbackPercentLabel":"of people found this helpful","captcha":{"error":"Please tick the box"}}}
Search FAQs

PowerChute Network Shutdown cannot be installed on 32-bit systems

Issue:
PowerChute Network Shutdown v4.3 and higher (v4.3+) cannot be installed on 32-bit systems.


Product Line:
PowerChute Network Shutdown

Environment:
All supported OS

Cause:
PowerChute v4.3 is bundled with JDK 11, which does not support 32-bit systems.

Solution:
If you require PowerChute on a 32-bit system, install PowerChute Network Shutdown v4.2, which is the last version to support 32-bit systems. To download PowerChute v4.2, visit the PowerChute Network Shutdown Product Page.

PowerChute v4.2 will continue to be supported 12 months after the release of v4.3, i.e. January 2020. For more information, see Knowledge Base article FA159606.
 

Can't find what you are looking for?

Reach out to our Customer Care team to receive information on technical support, assistance for complaints and more.