{}

Search FAQs

{"searchBar":{"inputPlaceholder":"Search by keyword or ask a question","searchBtn":"Search","error":"Please enter a keyword to search"}}

Using the StruxureWare DCE Linux internal browser to launch to devices causes an error when the DCE client is installed on some Linux systems.

Article available in these languages: Russian

Issue:
Using the StruxureWare DCE Linux internal browser to launch to devices causes an error when the DCE client is installed on some Linux systems.

Product Line:
StruxureWare Data Center Expert

Environment:
Linux
StruxureWare Data Center Expert version 7.x

Cause:
This issue is known to occur on some Linux systems when the internal browser is used to automatically log in to the web interface of devices that use basic authentication.

Resolution:

In the StruxureWare DCE client, uncheck the option to Use the Internal Web Browser when Launching to Devices in Browser Settings, accessed from the Client Preferences in the File menu.
Note: You must now manually log in to devices that use basic authentication.

Did this answer your question?

Explore more
Explore more
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.