{"support":{"yesButton":"yes","noButton":"no","feedback":{"title":"What can we do to improve?"},"submitButton":"Submit","successMessage":"Thank you for your feedback","title":"Did this answer your question?","feedbackPercentLabel":"of people found this helpful","captcha":{"error":"Please tick the box"}}}
Search FAQs
{"searchBar":{"inputPlaceholder":"Search by keyword or ask a question","searchBtn":"Search","error":"Please enter a keyword to search"}}
Alert Actions for NetBotz Version 2 and 3 Appliances
Issue:
Alert Actions for NetBotz Version 2 and 3 Appliances
Product Line:
Netbotz
Environment:
NetBotz Version 2 and 3 appliances
Cause:
The NetBotz Version 2 Appliances (320, 420, 500) support a variety of alert actions. Version 3 4xx and 5xx NetBotz also support these alerts based on configuration / connections. Some of these alert actions are only applicable if the required hardware and/or software is available. The following table defines the available alert actions and required hardware.
Resolution:
Note: Refer to the NetBotz documentation for configuring the prerequisite hardware and software.
Alert Actions for NetBotz Version 2 and 3 Appliances
Product Line:
Netbotz
Environment:
NetBotz Version 2 and 3 appliances
Cause:
The NetBotz Version 2 Appliances (320, 420, 500) support a variety of alert actions. Version 3 4xx and 5xx NetBotz also support these alerts based on configuration / connections. Some of these alert actions are only applicable if the required hardware and/or software is available. The following table defines the available alert actions and required hardware.
Resolution:
Alert Action | Results | Prerequisites |
---|---|---|
Send Email | Sends an email via SMTP to one or more target recipients | none |
Send Short Message Email | Sends a custom formatted email via SMTP to one or more target recipients | none |
Send SMS Message | Sends an SMS text message via GSM service provider | GPRS / GSM Wireless Adapter |
Send SNMP V1 Trap | Sends an SNMP version 1 trap to configured targets | none |
Send HTTP POST | Sends standard (all) alert information formatted in XML to a web server in the form of an HTTP POST | Properly configured web server and application code |
Send Custom HTTP Get | Sends customized alert information to a web server in the form of an HTTP GET | Properly configured web server and application code |
Send Data to FTP Server | Sends standard alert data formatted in XML to an FTP server. | Properly configured FTP server |
Send Custom Text File to FTP Server | Sends custom alert text file to an FTP server | Properly configured FTP server |
Set Switch Output State | Sets the state of an device switch | Supported output device such as Output Relay Pod, Power Control Pod or third party intelligent power strip |
Activate Button State | Activates a push button defined on an output device | Supported output device such as Output Relay Pod, Power Control Pod or third party intelligent power strip |
Play Audio Alert | Plays or speaks the text of the alert | NetBotz 500, Camera Pod 120 and attached external, power speakers |
Call Web Services Alert Receiver | Sends customer alert information via the Web Services API to a remote system | Properly configured web server running custom application code integrated with the NetBotz Web Services API |
Note: Refer to the NetBotz documentation for configuring the prerequisite hardware and software.
Explore more
Explore more
Can't find what you are looking for?
Reach out to our Customer Care team to receive information on technical support, assistance for complaints and more.