Browse FAQs

The ACRP-DX use the R407C refrigerant, is it possible to use the R410A instead of R407C?

Published date: 03 September 2020

Issue:
This document contains information about the ACRP-DX use the R407C refrigerant, is it possible to use the R410A instead of R407C?
 
Product line:
ACRP100, ACRP101, ACRD500, ACRD501, ACRD600, ACRD601, ACRD600P, ACRD601P
 
Environment:
All Serial Numbers
 
Cause:
Install, Repair
 
Resolution
 
Systems designed for R410A are designed at higher condensing temperatures and are not interchangable with R407C refrigerant.

Any conversion is not supported for any type of unit.


 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.