Technical FAQs

Ask a Question

Filter results

    Can the horizontal cable troughs ar8008blk and ar8016ablk be used in conjunction with vertical cable managers ar7580a, AR7585 and AR7588?
    ... on the horizontal cable troughs will mount ... the rails when vertical cable managers ar7580a, AR7585 ... NetShelter SX Wide cabinets, vertical cable management and horizontal ... All 750mm wide NetShelter SX cabinets: ar7580a ... ... to use both vertical finger-style vertical cable managers and horizontal cable troughs on the ... rails of a 750mm wide NetShelter SX cabinet. ... , when using vertical cable managers such as ar7580a ... still install the cable troughs which run ... ... holes in the cable managers and prevent hot ...
    Can the vertical cable management fingers for 600mm wide NetShelter cabinets be installed into 750mm wide NetShelter cabinets?
    ... AR7723 into a wide NetShelter SX or SV. NetShelter SX and SV ... shows that these cable managers are not compatible with the wide SX or SV cabinets ... ... installed into a 750mm wide cabinet. ... for the 600mm wide NetShelter SX cabinets, so ... with the 600mm wide cabinets only. In the SX cabinets a better choice may be the ar7580a (42U), AR7585 (45U) or AR7588 ( 48U ) because they offer far more capacity. In the SV cabinets AR7721 and AR7723 are currently the only finger-style vertical cable managers available.
    Can the horizontal cable side channel organizer be installed into a 600mm wide NetShelter SX, VX or SV cabinet?
    ... mounting rails of NetShelter SX 750mm wide cabinets. NetShelter Cable Management ... need to move cables horizontally from front ... in a 600mm wide NetShelter cabinet. ... the narrower 600mm wide NetShelter cabinets when paired with a cable manager like ar8603a. ... The ar8603a has two large brush- ... sections that allow cables to feed through ... ... support up to two of the cable side channels. (4 cable side channels total ... ... of the cabinet cable side channels can ... ... notice that the cable manager will interfere with ...
    How many cables can fit into a vertical or horizontal cable manager, or through an opening in a NetShelter cabinet?
    Customers need to know approximately how many cables will fit into specific cable management products. ... NetShelter SX , NetShelter Cable Management ... Need to manage cables neatly in a cabinet or rack. ... The document attached below shows estimated fill rates for various APC cable management products and openings in NetShelter cabinets. The estimates take into account the outer diameter of the cable and fill ratio. ... Fill ratio is the percentage of available space that's unused because there are air gaps between the cables . ... There are two files attached below:
    When finger-style vertical cable managers are used is it possible to also block off the openings in the mounting rails?
    ... finger-style vertical cable managers inside a NetShelter cabinet wants to ... NetShelter SX ... finger-style vertical cable managers to allow cables to run from ... When there are finger style cable managers installed inside the cabinet, AR7714 can be used as a pass-thru airflow management accessory. The AR7714 installs onto the finger style vertical cable manager . ... Without the finger-style vertical cable managers in place, ar7706 can be used in the wide NetShelter cabinets. It's a brush strip style airflow management product that allows cables to pass through. It installs onto the vertical mounting rail.
    Can vertical cable managers or 0U accessory rails be installed in the front and rear of a NetShelter SX cabinet?
    Issue: Customers want to know if there is flexibility in installing vertical cable managers , or where to mount the 0U accessory rails.
    Is it possible to convert a NetShelter SX Networking cabinet into a standard NetShelter SX cabinet?
    ... a cabinet from NetShelter Networking to NetShelter SX ? NetShelter SX and Networking cabinets ... customer has a NetShelter Networking cabinet and ... to a standard SX cabinet. ... to convert a NetShelter Networking cabinet into a NetShelter SX cabinet. ... all four existing vertical mounting rails, ... finger-style cable managers in the front ... Replace the vertical mounting rails. ... choose the correct SX full height rails ... ... large quantities of cables . ... you'll find the NetShelter SX roofs in the NetShelter Compatibility Chart. ... to modify a NetShelter SX cabinet into a NetShelter Networking cabinet.
    Results 1 - 10 of 50