Browse FAQs

Can the NetShelter AV busbar be installed into other NetShelter cabinets?

Published date: 21 February 2020

Issue:
AR8395 mounts to the accessory rail in the cabinet so it should be able to install into any NetShelter cabinet. 

Product Line:
AR8395

Environment:
All versions and serial ranges.

Cause:
AR8395 description says that it's for the NetShelter AV cabinets. 

Resolution:

The AR8395 can be installed into any NetShelter cabinet that has 20U vertical mounting space available. 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.