MGE PMM; Where can I find Modbus RJ45 connector label and wiring correction
Published date:
15 July 2020
Issue: Modbus RJ45 connector label and wiring correction
Product line:
PMM 400 / PMM 500
Environment:
PMM 400 / PMM 500
Cause:
Modbus RJ45 connector 4-wire diagram has RXD wiring labeled incorrectly base on the wiring harness connected to the NMC interface board. Also, note that the example below shows the master controller wired to the RJ485 Modbus connector TX to TX and RX to RX. Normally the Modbus controller to the device the TX would go to RX and RX to TX, but the wiring hardness does this Modbus controller swamp.
Resolution: Below highlight the corrections to connector/wiring for a Modbus controller to the PMM.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.