Technical FAQs

Ask a Question

Video: How to view alarms on an ACRD200 cooling unit

Issue:
How View Alarms on an ACRD200 Cooling Unit.

Product line: 
InRow Cooling Products ACRD200.

Environment:
All Serial Numbers.

Cause:
Install, Configuration

Resolution:



First you need to access the View Alarms menu you can do this by hitting the <ESC> until visible
 
Then select ENTER
 
You will be prompted for a Password if limited access is enabled
 
Use the default password of “apc”
 
If this does not work check with your Admin for the correct password
 
If password has been lost use the last eight digits of the serial number
 
Using the Up and or Down Arrows you can scroll through the alarms
 
 
 
Was this helpful?
What can we do to improve the information ?