All firmware versions (unless otherwise specified)
All serial numbers
Cause
This compatibility chart has been created for reference.
Resolution
Please refer to the table below.
Note: Some of these management cards are older and discontinued. This means while there may be some compatibility between current UPS models and discontinued management cards, support for new device features or management card features and bug fixes will only be available with the current generation of Network Management Card for your device. Current generation Network Management Cards purchased on their own will ship with the SUMX application file, for use with the Smart-UPS family. Firmware files for use in other UPS systems can be found here: https://www.apc.com/us/en/tools/download/ (Filter by Software/Firmware and choose "Firmware Upgrade")
Network Management Card Model(s)
UPS Model
Note(s)
AP9640, AP9641
Single and Three Phase Smart-UPS with the following model prefixes:
SUA*
SUM
SURT
SURTA
SURTD
SUVT & MGE Galaxy 3500
SMT
SMTL
SMX
SRT
SRTL
SRC
Symmetra LX (Single phase Symmetra UPS)
*Note: SUA devices manufactured after 2008. With Firmware version v1.4.2 and above, supported added for some SmartUPS 3.6G models: SUA750RM1U, SUA1000RM1U, SUA750RMI1U, SUA1000RMI1U, and SUA750RMJ1UB
AP9644
Three Phase Galaxy UPS units:
Galaxy VS*
*Includes built-in network management card.
Notes:
The AP9644 card is supported on the Galaxy VS from UPS firmware version 6.31.3.x.
The AP9644 card is backward compatible with any Galaxy VS already installed. When the card is installed after the UPS, however, a new Start-up service (WSTRTUP-VS1-A50) needs to be purchased to upgrade the UPS and the card at the customer site.
AP9630/30CH, AP9631/31CH
Single and Three Phase Smart-UPS with the following model prefixes:
SU
SUA
SUM
SURT
SURTA
SURTD
SUVT & MGE Galaxy 3500
SMT
SMX
SRT
SRC
Matrix UPS with UPS firmware versions Y or Z
MX3000
MX5000
Single phase Symmetra models:
Symmetra Power Array
Symmetra RM
Symmetra LX
Three phase Symmetra models:
48kW Symmetra PX2 All-In-One*
20kW Symmetra PX
40kW Symmetra PX
80kW Symmetra PX
100kW Symmetra PX2*
160kW Symmetra PX2*
SMX/SMT require sumx APP v5.0.3 or higher.
SRT models require sumx APP v6.0.7, or v6.2.0 or higher
*Note: This add-on option is only able to monitor the UPS, and not any power distribution. The embedded NMC within the UPS must be used to monitor any power distribution.
AP9630/30CH, AP9631/31CH, AP9635/35CH
Three Phase Galaxy UPS units
Galaxy 300/7000*
Galaxy VM
*Ships with AP9630 pre-installed in units manufactured post 2012. Older G7000 models require a special upgrade kit pre-2012 manufacture date.
AP9635/35CH
3 Phase UPS models including:
Symmetra PX 250/500
SUVT/G500*
Symmetra PX 20/40/80
Symmetra PX2 48kW All-in-One*
Symmetra PX2 100/160 kW*
Single Phase UPS models including:
Smart-UPS*
Symmetra*
*With AOS 6.4+ only, modem features only supported on MGE Galaxy units
**When using a NMC with an embedded NMC/Brain the FW file revisions must match. IE. 6.50 with 6.50, 6.8 with, 6.8, etc. Failure in doing so will cause communication alarms and display malfunction.
G5K9635CH
MGE Galaxy 5000
Kit includes all necessary parts to install an AP9635 for all G5000 UPS serial numbers and firmware.
G9K9635CH
MGE Galaxy 9000
Kit includes all necessary parts to install an AP9635 for all G9000 UPS serial numbers and firmware.
AP9617, AP9618, AP9619
Single and Three Phase Smart-UPS with the following model prefixes:
SU
SUA
SUM
SURT
SURTA
SURTD
SUVT*
Matrix UPS with UPS firmware versions Y or Z
MX3000
MX5000
Single phase Symmetra models:
Symmetra Power Array
Symmetra RM 6K/12K
Symmetra LX
Three phase Symmetra models:
20kW Symmetra PX All-In-One
40kW Symmetra PX
80kW Symmetra PX
100kW Symmetra PX2**
160kW Symmetra PX2**
Silcon
*Note: SUVT model UPSs with v7.X.X firmware should use NMC2 to take advantage of all UPS firmware enhancements.
**Note: This add-on option is only able to monitor the UPS, and not any power distribution. The embedded NMC within the UPS must be used to monitor any power distribution.
AP9606
Older UPS models including:
Smart-UPS with the following model prefix:
SU
SUA
Symmetra Power Array
Symmetra RM 6K/12K
Matrix UPS with UPS firmwares Y or Z
MX3000
MX5000
40kW Symmetra PX
80kW Symmetra PX
Silcon
0J-0N-9581GVM
Galaxy VM
Spare part for Galaxy VM Display/Embedded Network Management Card inside
0G-9354
W0G-9354 (spare part)
0G-9354A
0J-0G-9354A (spare part)
Three phase Symmetra (PX2) models:
48kW Symmetra PX All-In-One
100kW Symmetra PX
160kW Symmetra PX
UPS brain with embedded Network Management Card.
"A" SKU's are built on NMC2 architecture
Note: Certain features are limited by application.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.