Technical FAQs

Ask a Question

What happens to a Heat Exchanger if there is debris in the water, or high mineral content?

                                                                                                                                                         

Issue:  
What happens to a Heat Exchanger if there is debris in the water, or high mineral content? 

Product line:
Network Air FM, ACRD200, Uniflair Multi-Cool. 

Environment:
All Serial Numbers. 

Cause:  
Blockage. 

Resolution:  

 

 

Pic. 1: Completely blocked channels secondary side (water-side)

 

 

Pic. 2: Copper corrosion secondary side (water-side)

 

 

Pic. 3: Completely blocked channels secondary side (water-side)

 

 

 

 

 

 

 

 

 

 

Was this helpful?
What can we do to improve the information ?