What is the flow rate required for the InRow ACRD2XX fluid-cooled unit?
Published date:
03 September 2020
Issue:
This document answers the question of what is the flow rate required for the InRow ACRD2XX fluid-cooled unit?
Product line:
ACRD2XX.
Environment:
All systems.
Cause:
Normal operation and configuration.
Resolution:
Each InRow RD fluid-cooled unit requires a flow rate of 10gpm within its loop. This is for a single RD piped to a single outdoor fluid cooler. The flow rates will vary for custom configurations consisting of multiple RD units to a single outdoor dry cooler. Additional guidance on flow rates can be obtained from the Applications Engineering team.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.