Consultar las preguntas frecuentes



Hardwiring to 120v, 208v, and 240v loads from a 208v/240v SmartUPS RT UPS
... 240v SmartUPS RT UPS Smart- UPS RT ... "T" in the suffix of ... ... This does * NOT * ... units and do not require a stepdown ... Smart- UPS RT units designed for 208v/240v ... ... 240v Smart- UPS RT is a single phase UPS with a 3 ... They do not use a neutral ... ... stepdown transformer to power 120v loads and ... ... output of the UPS is unbalanced, ... will see 208 volts (or 240v ... however it is not two balanced 120 volt legs as you ... /240v utility power . ... 240v via the network management card or ...
What are the basic troubleshooting steps for the Smart-UPS smx2000hv / smx3000hv ?
... Cause Solution The UPS will not turn on or ... The unit has not been turned on ... ... turn on the UPS . ... even though the UPS is OFF. The UPS is not connected to utility power . ... sure that the power cable is securely ... to the utility power supply. ... load to the UPS , disconnect nonessential ... ... no input utility voltage Check the utility power supply to the UPS by plugging in a table lamp ... ... check the utility voltage . ... connector plug is not securely connected. ... is an internal UPS fault.
What are the basic troubleshooting steps for the Smart-UPS smx2000lv / smx3000lv ?
... Cause Solution The UPS will not turn on or ... The unit has not been turned on ... ... turn on the UPS . ... even though the UPS is OFF. The UPS is not connected to utility power . ... sure that the power cable is securely ... to the utility power supply. ... load to the UPS , disconnect nonessential ... ... no input utility voltage Check the utility power supply to the UPS by plugging in a table lamp ... ... check the utility voltage . ... connector plug is not securely connected. ... is an internal UPS fault.
What are the basic troubleshooting steps for the Smart-UPS smc1000 / smc1500 ?
... Cause Solution The UPS will not turn on or ... The unit has not been turned on ... ... turn on the UPS . ... even though the UPS is OFF. The UPS is not connected to utility power . ... sure that the power cable is securely ... to the utility power supply. ... load to the UPS , disconnect nonessential ... ... no input utility voltage Check the utility power supply to the UPS by plugging in a table lamp ... ... check the utility voltage . ... connector plug is not securely connected. ... is an internal UPS fault.
What are the basic troubleshooting steps for the Smart-UPS smx2000rmhv2u / smx3000rmhv2u ?
... Cause Solution The UPS will not turn on or ... The unit has not been turned on ... ... turn on the UPS . ... even though the UPS is OFF. The UPS is not connected to utility power . ... sure that the power cable is securely ... to the utility power supply. ... load to the UPS , disconnect nonessential ... ... no input utility voltage Check the utility power supply to the UPS by plugging in a table lamp ... ... check the utility voltage . ... connector plug is not securely connected. ... is an internal UPS fault.
What are the basic troubleshooting steps for the Smart-UPS smx2000rmlv2u / smx2200rmlv2u / smx3000rmlv2u ?
... Cause Solution The UPS will not turn on or ... The unit has not been turned on ... ... turn on the UPS . ... even though the UPS is OFF. The UPS is not connected to utility power . ... sure that the power cable is securely ... to the utility power supply. ... load to the UPS , disconnect nonessential ... ... no input utility voltage Check the utility power supply to the UPS by plugging in a table lamp ... ... check the utility voltage . ... connector plug is not securely connected. ... is an internal UPS fault.
What are the basic troubleshooting steps for the Smart-UPS smc1000-2U / smc1500-2U ?
... Cause Solution The UPS will not turn on or ... The unit has not been turned on ... ... turn on the UPS . ... even though the UPS is OFF. The UPS is not connected to utility power . ... sure that the power cable is securely ... to the utility power supply. ... load to the UPS , disconnect nonessential ... ... no input utility voltage Check the utility power supply to the UPS by plugging in a table lamp ... ... check the utility voltage . ... connector plug is not securely connected. ... is an internal UPS fault.
Video: How do I configure a 208v Smart-UPS RT or SRT for use with a 240v input?
If you need 120 v for your equipment you will still need to use a stepdown transformer.
What are the basic troubleshooting steps for the Smart-UPS smx1500rm2u ?
If the UPS indicates a site wiring fault, have a qualified electrician inspect the building wiring. (Applicable for 120 V units only.)
What are the basic troubleshooting steps for the Smart-UPS smx750 / smx1000 / smx1500 ?
If the UPS indicates a site wiring fault, have a qualified electrician inspect the building wiring. (Applicable for 120 V units only.)


Resultados 1 - 10 de 63

¿No encuentras lo que buscas?

Ponte en contacto con nuestro equipo de atención al cliente para obtener información sobre asistencia técnica, asistencia para quejas, etc.