{}

Buscar Preguntas Frecuentes

{"searchBar":{"inputPlaceholder":"Busca por palabra clave o haz una pregunta","searchBtn":"Buscar","error":"Ingresa una palabra para buscar"}}

Network Management Card 660674/34003640SE; Ripple20 vulnerability status

Issue:
Ripple20 vulnerability status



Product line:
660674/34003640SE Network Management Card (NMC)


Environment:
660674/34003640SE Network Management Card (NMC)


Cause:
Information about the 66074 NMC and the Ripple20 vulnerability (Treck Inc.’s embedded TCP/IP stack).


Resolution:

The 66074 NMC does not use the Treck Inc.’s embedded TCP/IP stack for TCP/IP but use a inhouse TCP/IP stack developed by the NMC vendor.  This NMC is not affected by this vulnerability.


¿Te fue de ayuda?

Explora más
Explora más