{}

Nuestras marcas

{"support":{"yesButton":"Sí","noButton":"No","feedback":{"title":"¿Qué podemos hacer para mejorar?"},"submitButton":"Enviar","successMessage":"Gracias por tus comentarios","title":"¿Te fue de ayuda?","feedbackPercentLabel":"de las personas encontraron esto útil","captcha":{"error":"Por favor, marca una casilla"}}}

Buscar Preguntas Frecuentes

{"searchBar":{"inputPlaceholder":"Busca por palabra clave o haz una pregunta","searchBtn":"Buscar","error":"Ingresa una palabra para buscar"}}

NetBotz 355 | Physical Description

Issue:
Physical Description of the NetBotz 355 and 355A

Product Line:
NetBotz version 3
- Wall Monitor 355
- Wall Monitor 355A

Environment:
NetBotz 355/355A (all firmware versions)

Resolution:

Physical Description - Front



ItemDescription
1Vented internal sensorsVented opening for airflow, temperature, and humidity sensors.
2Network link LEDShows the status of the network connection. Blinks to indicate network traffic (green = connected at 10 Mbps; yellow = connected at 100 Mbps).
3Power LEDIndicates whether the unit is receiving power (green = receiving power; dark = not receiving power)
4Camera LEDBlinks steadily when the integrated camera is active.
5Alert LEDIndicates the alert status of the system.  When more than one alert exists, the most severe will be indicated.
- Flashing once every eight seconds = Informational
- Flashing one very four seconds = Warning
- Flashing once every two seconds = Error
- Flashing once every second = Critical
- Flashing twice per second = Failure
6Temperature display- Displays the current temperature from 0 to 99 in Centigrade or Fahrenheit. The Temperature reading comes from the internal temperature sensor. If the temperature exceeds 99, the display will flash 99.
- When the unit first receives power, displays the unique identifier number for one minute.
- If an alert exists, flashes at the same rate as the Alert LED.
- During firmware upgrade, displays 88.
7Lens housingMust be removed to change the focus of the integrated camera.

Physical Description - Back
ItemDescription
1Sensor ports (4)Used for connecting APC by Schneider Electric sensors, third-party dry-contact sensors, and standard third-party 0-5 V sensors. Third-party dry-contact state sensors require the NetBotz Dry Contact Cable (NBES0304). Standard third-party 0-5 V sensors require the NetBotz 0-5 V Sensor Cable (NBES0305).
210/100 Base-T network portProvides for a 10/100 Base-T network connection and power through Power-over-Ethernet (PoE). (The appliance operates at 100 Base-T only.) Status and link LEDs indicate network traffic:
- Status LED: blinks orange and green at start-up, then indicates the status of the network connection (solid green = IP address established; blinking green = attempting to obtain an IP address).
- Link LED: blinks to indicate network traffic (green = connected at 10 Mbps; orange = connected at 100 Mbps).
3USB portUsed to configure the appliance.
4ResetUsed to restart the appliance.

The complete NetBotz 455 Installation and Quick Configuration Manual can be found here.
Explora más
Explora más

¿No encuentras lo que estás buscando?

Comunícate con nuestro equipo de Atención al Cliente para recibir soporte técnico, asistencia para quejas y más.