Browse FAQs



Why does ISX Manager/StruxureWare Central display the incorrect Kilowatt value when utilizing the Physical Layout or ISX Operations feature for my Metered/Switched Rack PDU product?
... or ISX/ StruxureWare Operations tools from my Metered or Switched Rack PDU. ISX Operations StruxureWare Data Center Operations ... and AP88XX Metered Rack PDUs ... Metered By Outlet Rack PDUs ... and AP86XX Metered Rack PDUs ISX or StruxureWare Operations - All Versions ... Physical Layout or StruxureWare Central Operations to display the ... ... (AP79XX) Rack PDU's as well ... ) that have 3 .X. ... ISX Manager or StruxureWare Central via SNMP ... Physical Layout or StruxureWare Operations tool. ... /or Switched Rack PDU and inline ... Alternatively, these values can be changed via SNMP on most prior rpdu APP revisions.
Data Center Expert | How do hardware and software support contracts work?
Cause: StruxureWare Data Center Expert appliances come with 2 years of factory hardware warranty and no
What is the maximum number of rack access cards that can be configured in a version 3 NetBotz appliance for use with the rack access pod 170?
When using StruxureWare Data Center Expert to configure multiple NetBotz appliances, the limit in this system is also 200 cards and again all cards ...
Video: Data Center Expert | Desktop Client Requirements, Download, & Installation
The StruxureWare Data Center Expert Desktop Client (console) is a stand -alone Java application that runs on systems that meet the following ...
NetBotz v3 | How do I configure location settings?
StruxureWare Data Center Expert will only pull in the main location field of the Sensor Pods, Rack Access Pods, and wireless devices to ...
Video: Data Center Operation | Copying files from the StruxureWare Data Center Operation
How to copy files from the StruxureWare Data Center Operation ... StruxureWare Data Center Operation ... StruxureWare Data Center Operation (All Versions) ... Files such as backup and logs can be "downloaded" from the Operation server using SFTP/FTP. In this document, we will be using a free program called WinSCP. You can find this program . ... 1. Open the application ... 3 . Enter log in credentials in both "Username" and "Password" fields ... 1. Double click on data folder ... 3 . Locate the backup to save off server
Data Center Expert | Why does StruxureWare not accept my One Time passcode?
StruxureWare Data Center Expert is not ... StruxureWare Data Center Expert (DCE ... StruxureWare Central (SWC ... StruxureWare Data Center Expert (all ... StruxureWare Central (all ... SturuxureWare Data Center Expert requires a ... passcode and the Data Center Expert's MAC address ... StruxureWare Data Center Expert (DCE ... ... to gather specific information about the alert ... 3 . If you ... AP9465 = StruxureWare Data Center Expert Basic ap9470 = StruxureWare Data Center Expert Standard AP9475 = StruxureWare Data Center Expert Enterprise AP94VMACT = StruxureWare Data Center Expert Virtual Machine SFDCOBASE = StruxureWare Data Center Operation ... a VM or Data Center Operation .
Data Center Expert | How can I resolve “Failed to create java virtual machine.” error when launching StruxureWare Data Center Expert client?
... Upon launching the StruxureWare Data Center Expert client an ... StruxureWare Data Center Expert (DCE ... StruxureWare Central (SWC ... StruxureWare Client (potentially ... StruxureWare may be attempting ... ... Installation directory for StruxureWare Data Center Expert. ( ... C:\ Program Files (x86)\ StruxureWare Data Center Expert X. ... 3 ) Within the dcexpert directory open the jre directory and then the bin directory. ... -vm "C:\ Program Files (x86)\ StruxureWare Data Center Expert 7.2.7\dcexpert\jre\bin\javaw.exe"
File transfers may be unsuccessful using SCP on devices within StruxureWare Data Center Expert (DCE) with v6.X.X firmware earlier than v6.3.3
... using SCP within StruxureWare Data Center Expert may be ... ... NMC2 such as Rack PDU StruxureWare Data Center Expert ... the device through StruxureWare Data Center Expert, you ... ... enabled devices and applications . You can do this within StruxureWare under the Updates->Apply Firmware Updates screen within the DCE client. ... If using StruxureWare DCE for this configuration, make sure to set the correct "Device File Transfer Settings” options in DCE before you select the v6.X.X devices you want to update.


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.