Browse FAQs



APC Schneider Cooling Unit Identification
APC Cooling Unit identification. All Cooling Units . APC Unit Identification E= Expansion A= Air Cooled E= Air Cooled ... Humidifier D= Downflow ... Humidifier D= Downflow ... Main A= Air Cooled ... Humidifier D= Downflow ... ) A= Air Cooled D= Downflow ... ) A= Air Cooled DF= Downflow ... ) A= Air Cooled E= Air Cooled w/Multicool R= Air Cooled w/Remote ... ... -5T Air Cooled or ... 0 A= Air Cooled SC= Air Cooled Self-Contained IR= Air Cooled Indoor Condenser
Why do I need refrigerant traps in my piping?
All Air Cooled Cooling Units ... Oil is easily trapped in a discharge muffler, so it should be placed in the horizontal or downflow portion of the piping, as close to the compressor as possible. ... A: Whenever a condenser is located above the compressor, an inverted trap or check valve should be installed at the condenser inlet to prevent liquid refrigerant from flowing backwards into the compressor during off cycles.
Network Air FM fan curve chart
Issue: Network Air FM fan curve chart.
DAC, Cancoil Installation Manual
Cancoil air-cooled condensers are available ... variety of optional fan cycling controls, however many units are shipped without fan controls. Check the unit wiring diagram for ...
What are the operational conditions for an InRoom (Stulz) Unit
This document will describe what are the operational conditions for an InRoom (Stulz) Unit . ... The InRoom precision air conditioning units operate within the following ranges: ... Maximum equivalent length of piping between the cooling unit and the air cooled condenser: 60 m (200 ft) Maximum level difference between the condenser and the cooling unit : 5 m (16 ft) when the condenser is below the cooling unit ... Downflow units with an external static pressure: 20 Pa (0.08 in w g)
How to navigate through an Network Air FM unit display
... Network Air FM unit display. Direct expansion (DX) ... When the unit is in dehumidification ... ... All refrigerant is directed through the expansion valve which feeds ... ... used in the direct expansion refrigeration system. ... ... begins when an Expansion Module loses communication ... ... expires, the Expansion Module will shut ... ... or set the Expansion Modules to continue ... ... mode to the direct expansion coil. —for air-cooled Modules with no MultiCool coil. ... Air-cooled Systems with no external water piping do not require a condenser valve actuator.
General functions of a MicroAC control platform DG3
The MicroAC is an electronic control for the complete management of precision air-conditioners, both in direct expansion versions (with 1 or 2 compressors), with 1 or 2 heating elements or with batteries (valve on the heating battery and/or valve on the cooling battery). ... In addition, it can also be used in precision units for "Shelters" with management of the condenser fan .
Where can I get support for APC and MGE Products?
Air Cooled Chillers ... Environmental Monitoring Unit ... InRoom Direct Expansion ... InRow Direct Expansion
How to clean Heatcraft-Larkin Refrigeration condensers
Air cooled condensing units require a minimum of maintenance. The unit coil will require a periodic cleaning and this can be accomplished by a brush, vacuum cleaner, pressurized airstream or a commercially available coil cleaning foam. All of the condenser fan motors have sealed ball bearings.
What should be checked if the NetShelter CX internal temperature exceeds expected levels? (5*C/41*F above room temp)
Fan issues, air ... 1. Check the fan trays and make sure all the fans are powered and working correctly. 2. Check that the foam clamp is fastened tightly around the cables exiting the cabinet otherwise air will be drawn through the gap and straight into the air inlets of the fan modules, thus bypassing the internal equipment. ... There should be a gap of 200 mm (8") on each side to allow warm air to exit the fan modules. 8. Make sure the cabinet is not positioned in direct sunlight.


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.