How to download and use the APC UPS-Link Protocol Language
Published date:
27 July 2020
Issue:
How to obtain APC UPS-Link Protocol language
Product Lines:
Smart-UPS, Matrix, Symmetra NOTE: The UPS-Link Protocol is used only for APC smart signaling UPS models. This UPS-Link Protocol does not support SMX/SMT/SURTD/SRT models or other next generation UPS's without the use of the AP9620 Legacy Communications Card (LCC).
Environment:
All OS
Cause:
Users who are running an operating system or application which APC does not provide a pre-developed software solution for can now download the UPS-Link language protocol from the APC web site free of charge.
Solution:
By clicking on "Download" the customer agrees to be bound by the Terms and Conditions of the Licensing Agreement which includes using the language for the purpose stated on the contract only. This Licensing Agreement is also available to download from the APC web site for review.