Consulter la FAQ

Modbus communication on a Uniflair unit.

Date de publication : 08 March 2019

Issue:  
Modbus communication on a Uniflair unit.

Product line:
Uniflairl.

Environment:
All Models and Serial Numbers.

Cause: 
Install.

Resolution:  
MODBUS RTU 

Scenario 1 

Modbus is a communication protocol very famous and used all over the world. It’s quite easy and not so structured.

•          It has been developed at the end of ’70 from Modicom

•          The communication is multidrop, with Master and Slaves

•          It is not used only with industrial application

•          Serial communication: RS232 or RS485 half duplex

•          Protocol type: Modbus RTU (1 byte = 2 exadecimal words) and Modbus ASCII (1 byte = 2 ASCII  words).

Configurable Baud rate (max 19200) 

 

 

scheda seriale 485OD121JEGateway

 

The units, all fitted with the serial card, are connected:

• each unit with the RS485 cable;

• last unit with the final resistor;

• first unit with the Gateway.

 

To realize a local net to be connected to a BMS working with Modbus, it’s necessary:

• 1 gateway LBM every 16 units;

• 1 serial card RS485 for every controller;

• 1 terminal line (120 Ω);

• PC for the gateway configuration.

 

Scenario 2

 

Unites fitted with pCO1, upCOxs

 

 

Solid_UTP4_Cat_5__Cat_5e_Cable         scheda seriale 485 

 

To realize a local net to be connected to a BMS working with Modbus, it’s necessary:

• 1 RS485 serial card for every controller;

• 1 terminal line (120 Ω);

• PC for the gateway configuration.

 

 

 

 

 

 

 

 

 


Cela vous a-t-il aidé ?

Que pouvons-nous faire pour améliorer l'information ?

Vous n'avez pas trouvé ce que vous cherchiez ?

Contactez notre équipe client pour obtenir des informations sur l'assistance technique, l'assistance dédiée aux réclamations et plus encore.