Consulter la FAQ



"Site Wiring Fault" message on Symmetra LX UPS Systems
... difference between the 2 phases (i ... . phase ( 1 ) reports 120v and phase ( 2 ) reports 105v ... UPS will indicate Site Wiring Fault but ...
What the limitations and acceptable allowance for tilting an ACSC?
The installation instructions ( page 5) specifically ... [see figure 1 ]. The ... [see figure 2 ], but it seems to ...
DNS may not work properly after firmware upgrade on Network Management Card 1 (NMC1) when using DHCP boot mode
... Network Management Card 1 (NMC1) ... ... Network Management Card 1 include (but ... Until a firmware fix is available, users can re-apply the DNS settings through one of two ways. 1 .) Navigate to the DNS settings page within the web UI and click apply, or ... 2 .) StruxureWare Data Center Expert users can push out a configuration template with the DNS server information from DCE's APC SNMP Device Configuration feature.
How to take the Single Galaxy 5000 UPS from normal operation to total power off using an external Maintenance Bypass Panel
How to take the Single Galaxy 5000 UPS from normal operation to total power off using an external Maintenance Bypass Panel. ... All models , all serial numbers ... Due to site maintenance, inclement weather, and other conditions, request come in for assistance with Powering Down the Galaxy 5000 UPS ... This procedure is for a single UPS with an external maintenance bypass panel. ... Step 1 : Touch any button on the display to wake it up. Step 2 : Push the Menu Button ... Turn off Q 1 Switch
Can I use the search functionality of StruxureWare Data Center Expert's web page to search for NetBotz serial numbers?
Can I use the search functionality of StruxureWare Data Center Expert's web page to search for NetBotz serial numbers? ... StruxureWare Data Center Expert 7.2 has a search feature on it's new web page that allows you to search for sensors and devices. One of the parameters that can be searched is serial number. On NetBotz version 2 appliances, the serial number is the same as the mac address.
PowerChute Business Edition Simple Signaling with Interface Expander 2 card in Timer Mode – Master server does not shutdown
... an Interface Expander 2 card using Timer ... ... with Interface Expander 2 card (AP9624 ... Option 1 : ... the Interface Expander 2 card from “ ... Option 2 : ... However, if the power outage does not last 2 minutes (Timer Mode setting on the Interface Expander 2 card), the Master server will still shut down. ... Visit on the APC website to find out more about UPS model types.
Rack PDU 2G (AP8XXX) Network Port Sharing Information
... AP8XXX Rack PDU models ... ability to share one IP address via one network connection) ... PDUs using only one ... a number, 1 to 4, ... After two or more Rack ... are connected to one another in a ... You'll need two terminators per Network ... ... which includes qty 2 terminators and provide ... ... " port of one of the grouped ... ... desired order, 1 to 4. ... ... have Display ID 1 . ... have Display ID 2 . Continue in ... ... power for phase 2 on guest Rack ... ... phReading 3: 2 power 2 : 40 W ... Group Status" page , and the ...
Reformatting a Version 2 or 3 Netbotz Appliance
... Reformatting a Version 2 or 3 Netbotz ... NetBotz Version 2 and Version 3 ... document explains the two methods used to ... a NetBotz V 2 /V3 ... Method 1 1 : Open a ... 2 : Use the ... ... message on the web page that says the ... Method 2 1 : If you have a V 2 appliance, use ... 2 : Start a ... ... Stop Bits: 1 ... netbotz (V 2 ) or root ... You can now close the serial communications program, disconnect your console cable, and log into the appliance using the default User ID and Password of netbotz (V 2 ) or apc (v3).
What to do if PowerChute Network shutdown configuration wizard displays blank Network Configuration page?
After installing PowerChute Network Shutdown when the configuration wizard runs the PowerChute Setup: Network Configuration page display is blank. ... 1 - stop PowerChute service ... 2 - Open pcnsconfig.ini using wordpad or notepad ... localHostAddress = 192.168. 1 .X ... mode = single IP_ 1 = 192.168.0.X ... 6 - After restarting PCNS1 service log into PCNS web page and select Shutdown Settings to complete the configuration.
Video: What does the Site Wiring Fault Indicator LED on my APC UPS or Surge Arrestor represent?
... What does the Site Wiring Fault Indicator ... ... equipped with a Site or Building Wiring ... The Site Wiring Fault ( ... ... your wiring for one or more of ... Reasons why the Site Wiring Fault (SWF) LED light will illuminate: ... (Note: this also includes using a 3 prong to 2 prong adapter) ... Therefore, in order to maintain your warranty and protection under APC's Equipment Protection Policy, be sure that the APC unit is only plugged into a properly grounded outlet where the Site Wiring Fault Indicator (SWF) light is not illuminated.


Résultats 1 - 10 de 71

Vous n'avez pas trouvé ce que vous cherchiez ?

Contactez notre équipe client pour obtenir des informations sur l'assistance technique, l'assistance dédiée aux réclamations et plus encore.