Consulter la FAQ



APC Schneider Cooling Unit Identification
P= Glycol Cooled w/Economizer C= Chilled Water BC=208-230/ 1 /60
Can cable bridge partition/trough be installed across the top of a 300 mm or 600 mm InRow chilled water cooling unit?
NetShelter troughs can span one cabinet width without attaching directly to the cooling unit roof.
Video: Clearing unit run hour violations on an Chilled Water Uniflair
Issue: Tis document describes how to clear Unit Run Hours Violation on Uniflair Chilled Water cooling systems .
Video: How to change a Cooling Set point on a push button Uniflair display
uniflair, chilled, water , push, button, display, cool, set, point, change, generation 1
What are the operational conditions for an InRoom (Stulz) Unit
... +/- 1 % Chilled water -/ cooling water pipes: Maximum water head pressure: ... ... piping between the cooling unit and the ... Maximum level difference between the condenser and the cooling unit: 5 m (16 ft) when the condenser is below the cooling unit ... Entering water temperature (EWT) for CW coil: 7°C (44.6°F) Leaving water temperature (LWT) for CW coil: 12°C (53.6°F) ... Cooling fluid (DX): 30% Glycol ... Chilled water medium (CW): 0% Glycol
Three Phase Power Products or Cooling Solutions One-Year Factory Warranty
Schneider Electric, UPS, Warranty, One - Year Factory Warranty,Warranty,Non-transferable Warranty
Are the fans in a 600mm Cooling unit single phase or 3-phase?
Issue: Are the fans in a 600mm Cooling unit single phase or 3-phase?
What alarms can be automatically reset on a High Capacity Uniflair Unit
• Low Pressure • Circuit 1 Chilled Water High Temperature Threshold Exceeded
Water leak in DataCenter.
... you find a Water leak on Indoor ... All DataCenter Cooling Units. All Product models , all serial ... ... , flush with water , or blow ... One of the very ... pour scalding hot water into it. ... and only has one trap. ... also cause the water to back- ... it doesn't have one . and is thawing, it may run water from nearly any place. ... clogs may cause the condensation water from the air conditioner to back up and overflow. Use the hot water tip above to clear it.


Résultats 1 - 10 de 96

Vous n'avez pas trouvé ce que vous cherchiez ?

Contactez notre équipe client pour obtenir des informations sur l'assistance technique, l'assistance dédiée aux réclamations et plus encore.