Consulter la FAQ



When multiple critical events occur, why does PowerChute Network Shutdown 3.0.1 not shut down using the shortest delay value in one of the events?
... of 300 seconds for event 1 and 120 seconds for event 2. If event 1 occurs first and ... shorter delay of 120 seconds.
USB Power Usage Guidelines for Netbotz
NetBotz USB Device Power Consumption The Sensor Pod 120 requires 1 point of power.
Temperature and Humidity Sensor Specifications for Version 1 Appliances
Temperature and Humidity Sensor Specifications for Version 1 Appliances ... NetBotz version 1 appliances ... Version 1 -- Appliance Temperature Sensor Specifications ... Range for all Version 1 Appliances (300, 303, 310, 400): ... 35 - 120 degrees F ... +/- 1 degree C ... Version 1 --Humidity Sensor Specifications Range:10% - 90 %, non-condensing ... Please note that Version 1 appliances are no longer supported.
Standard Lens Specifications for the WallBotz 500 & version 1 Camera Pod 120
Issue: Standard Lens Specifications for the WallBotz 500 & version 1 Camera Pod 120
Standard Lens Specifications for the WallBotz 500 & Camera Pod 120
Environment: NetBotz 500 / Camera pod 120 (Owl 1 pod only)
Uniflair SNMP (Simple Network Management Protocol)
Simple Network Management Protocol • 1 RS485 serial card for every control; 1 resistor ( 120 ω).
88 volts from the North American Symmetra Power Array output block
The output terminal block provides two 120 volt legs and one 88 volt leg.
Modbus communication on a Uniflair unit.
• 1 serial card RS485 for every controller; 1 terminal line ( 120 ω);
Lost Neutral - effects on loads and UL1449
240 VAC is used because most household wiring is 120 /240 3 wire single phase and a lost neutral produces 240 VAC.


Résultats 1 - 10 de 56

Vous n'avez pas trouvé ce que vous cherchiez ?

Contactez notre équipe client pour obtenir des informations sur l'assistance technique, l'assistance dédiée aux réclamations et plus encore.