Consulter la FAQ



What is AVR (Automatic Voltage Regulation)?
APC Back-UPS , APC Smart-UPS
Recommendations for protecting a laser printer
in to its Surge Only Outlets. These low voltage situations may cause an APC Back-UPS to transfer to battery operation repeatedly, ...
What are the differences between the Back-UPS RS and the Back-UPS XS models (Does not Include BX/BR LCD Models)
... 2. The Back-UPS RS models have ... features of Automatic Voltage Regulation ( AVR ), where as the Back-UPS XS only has ...
How to Brain Dead a Back-UPS unit. (Full UPS Logic Reset)
To brain dead a Back-ups is to purge the charge in the brain of the UPS. ... Back-UPS , Back-UPS Pro ... 2: Unplug the UPS from the wall socket . ... 4: Push and hold the ""On"" button on the UPS for 5 seconds 5 : Reconnect internal battery. ... http://www. apc .com/support/
Why might the LEDs on my Back-UPS or Smart-UPS SC be flashing?
... LED lights on Back-UPS Pro, Back-UPS Pro USB, Back-UPS LS, and ... Back-UPS Pro, Back-UPS USB, Back-UPS LS, Back-UPS CS, Back-UPS NS/XS ... ... included with your Back-UPS Pro after it ... ... from your wall socket . APC UPS Selector tool ... Each model of Back-UPS Pro is capable ... ... rated for 350 Volt Amps (or ... rated for 500 Volt Amps (or ... ... , please contact APC's Technical Support.
Video: Why might my APC Back-UPS Product be beeping?
- If the Frequency deviates + or - 5 % this will also cause a Back-UPS product to transfer to battery power.
What are some issues I may encounter when using an APC Back-UPS with a generator?
SOLUTION: APC recommends that Back-UPS units be desensitized ... more tolerant of voltage distortion and, therefore, make less transfers to battery ...


Résultats 1 - 10 de 62

Vous n'avez pas trouvé ce que vous cherchiez ?

Contactez notre équipe client pour obtenir des informations sur l'assistance technique, l'assistance dédiée aux réclamations et plus encore.