Environment: All Product models, all serial numbers
Cause: Units use dew point to calculate humidity
Resolution: You may come across an ACRP not generating an alarm message when the Return Humidity is lower than the Threshold [figure 1]. Remember Humidity set points and thresholds are based on dew point. It is possible to be under the RH% set point/threshold and not receive a humidity demand or warning.