Browse FAQs

What is the IP (Internal Protection) rating of the NetShelter SX, SV and CX cabinets?

Published date: 27 August 2020

Issue:
Internal Protection (IP) rating of the NetShelter SX, SV and CX cabinets is required.

Product Line:
NetShelter SX, NetShelter SV, NetShelter CX

Environment:
All versions and serial ranges.

Cause:

IP ratings are used to determine how large an object, or liquid, may pass through the side panels or roof of a cabinet.  For example a product that has a rating of IP44 when interpreted means that the product is protected against solid objects that are bigger than 1mm and water splashing from all directions.


Resolution:
 
NOTE: The NetShelter "AR" cabinets have not been independently tested to IEC 60529 standards for Internal Protection.

As stated above "cabinets have not been independently tested to IEC 60529 standards"
This includes: AR3100, AR3104, AR3107, AR3130, AR3140, AR3150, AR3157, AR3300, AR3305, AR3340, AR3347, AR3350, AR3357, AR3200, and AR3810, AR2400, AR2401, AR2400FP1, AR2480, AR2500, AR2580, AR2407, AR2487, AR2507, AR2587, AR2200, AR2280, 403AR4000MV, AR4018A, AR4018IA, AR4024A, AR4024IA, AR4038A, AR8IA.



 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.