What are the Condensate Pump lift specifications for your InRow product line?
Published date:
18 July 2020
Issue:
What are the Condensate Pump lift specifications for your InRow product line?
Product line:
All InRow Units
Environment:
Data Center Cooling
Cause:
Resolution:
All of the InRow products come with a factory-installed condensate pump piped internally to the condensate pan. Each pump has different specifications. If needed, more details can be found in the technical manual as well.
Charles Austen Pump - Capable of pumping 13.5 GPH (51 L/h) liquid a maximum distance of 65ft (20m) , which may include a maximum lift of 20 ft (7 m).*
Pacific Electronic - Capable of pumping 1.3 GPH (5 L/h) liquid a maximum distance of 50 ft (15.2 m), which may include a maximum lift of 16 ft (4.9 m).
NOTE: Dual floats are included with the unit. One float is used for condensate pump control, the other to generate condensate pan overflow alarms.