StruxureWare Central (SWC)
InfraStruXure Central (ISXC)
Environment:
StruxureWare Data Center Expert 7.x and earlier
Cause:
StruxureWare Data Center expert is a highly customized operating system.
Resolution:
StruxureWare Data Center Expert (DCE) is not supported as in install directly on any 3rd party hardware. There are specific drivers that are included in the system and we will not properly install on any hardware other than those sold by APC / Schneider Electric. Additionally, the install limits the amonts of devices that can be monitored based on the hardware on which it is installed.
If you must use 3rd party hardware, you can install VMware on that hardware and use the AP94VMTRL trial version of DCE and activate it using the AP94VMACT. With that, you have your own hardware as well as a supported system for running StruxureWare DCE in a virtual environment.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.