How much exhaust clearance is needed for a NetShelter CX cabinet?
Published date:
05 August 2019
Issue: The NetShelter CX may overheat if there is not proper clearance for airflow.
Product Line: NetShelter CX
Environment: All models and serial ranges.
Cause: Improper spacing can cause overheating.
Resolution :
See attached file.
NetShelter CX Wall Clearance
The exhaust fans of the NetShelter CX vent to the sides. The back of the cabinet can be placed against a wall if desired.
If the cabinet is being installed in a corner please leave at least 6 inches of open space between the side of the NetShelter CX and the wall.
It is not recommended to install a NetShelter S X where the back and both sides are against a wall.
Please see attached file for a graphic depiction of the clearance.