Technical FAQs

Ask a Question

NetBotz 250 | Reset Configuration to Defaults

Issue:
Process for resetting the configuration back to factory defaults on a NetBotz 250.

Product Line:
NetBotz 250 (NB250)

Environment:
NetBotz 250 (all versions)

Resolution:

1) Log into the NetBotz 250 web interface.
2) Control menu > Network > Reset / Reboot.
3) Select the reset method that best suits your needs:
- Reset All: all configured values and settings are reset to their default values, including the setting that determines how this device must obtain its TCP/IP configuration values. The default for that setting is DHCP.
- Reset All, exclude TCP/IP: All configured values and settings except the setting that determines how this device must obtain its TCP/IP configuration values are reset to their default values.
- Reset Only: TCP/IP, Event Configuration, Lost Communication Alarms, Temperature Rate Of Change Alarms, Module Configuration, and/or User Configurations.
 
Was this helpful?
What can we do to improve the information ?