Browse FAQs

What do the LED's on my Network Management Card mean?

Published date: 03 December 2020

Issue

The status and link LEDs (found on the left and right side of the ethernet port) on a Network Management Card give information on the current status of the NMC

Product Line
  • Network Manage ment Card 1 - AP9617, AP9618, AP9619
Devices with an embedded Network Management Card 1 include (but are not limited to): Metered/Switched Rack PDUs (AP78XX, AP79XX), Rack Automatic Transfer Switches (AP77XX, Environmental Monitoring Units (AP9320, AP9340, Netbotz 200)
  • Network Management Card 2 - AP9630/AP9630CH, AP9631/AP9631CH, AP9635/35CH
Devices with an embedded Network Management Card 2 include (but are not limited to): 2G Metered/Switched Rack PDUs (AP84XX, AP86XX, AP88XX, AP89XX), Certain Audio/Video Network Management Enabled products.
  • Network Management Card 4 – AP9644
Devices with an embedded Network Management Card 4 include: Galaxy VS
 
Environment 
  • All firmware versions (unless otherwise noted)
  • All serial numbers







Network Management Card 2



The status LED (right side facing) shows the following:

 
LED Behavior