StruxureWare Central (SWC)
InfraStruXure Central (ISXC)
Environment:
StruxureWare Data Center Expert Virtual Machine (VM) (All Versions)
Cause:
Assuming the backup being used to restore the new VM is not corrupt, if you import the backup to a system with the default size hard drive, it may not fully boot.
Resolution:
As per the local help files or the on-line help files for the VM found at:
www.apcc.com/tools/download
Migrating a StruxureWare Data Center Expert hardware server to a virtual appliance
Deploy the demo version OVA, and configure it using the hardware equivalents for the StruxureWare Data Center Expert Basic, Standard, or Enterprise server from which you are migrating. The available disk space for the virtual appliance must be greater than the disk space used by the hardware server.
Adding disk space to a virtual appliance
To increase storage for the virtual appliance, you must create additional hard disks. You cannot change the size of an existing hard disk, or remove a hard disk once it has been created. An error will occur on the primary interface, and the StruxureWare Data Center Expert virtual appliance will not start.
1. Gracefully shut down the virtual appliance.
2. In your virtual server console, select the option to add a hard disk.
3. Choose the hard disk size.
See StruxureWare Data Center Expert virtual server equivalent configurations.
4. Choose thin or thick provisioning.
5. Power on the virtual appliance.
Changes in the disk space will take effect once the StruxureWare Data Center Expert virtual appliance has restarted. Do not shut down the virtual appliance while the disk reconfiguration process is running.
The "Storage Settings" display, accessed from the Server Administration Settings option in the System menu, shows the total storage space available for the virtual appliance, not the individual hard disks.
Note: To store large amounts of surveillance data, using a remote repository is recommended.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.