Browse FAQs

What are the capabilities of the condensate pump on the ACSC unit?

Published date: 11 June 2020

Issue:
What are the capabilities of the condensate pump?
 
Product line:
ACSC100, ACSC101
 
Environment:
InRow Cooling
 
Cause:
 
Resolution:
The pump can remove 1.3 gal/hr (5.9 l/hr) at a maximum run of 50 ft (15.2 m) of which 16 ft (4.9 m) can be vertical lift. For example, if you have 10 feet (3 m) of vertical lift, you have 40 feet (12.2 m) left for usable horizontal run.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.