Browse FAQs

Smart-UPS VT-G3500; Why does my UPS report higher output current than input current?

Published date: 12 June 2020

 
 
 
Issue:
Why does my UPS report higher output current than input current?
 
Product line:
Smart-UPS VT-Galaxy 3500
 
Environment:
All model numbers, all serial numbers
 
Cause:
The UPS is rated for output power factor of 0.8, while the input is power factor corrected. The result is a lower input current than output current, as the difference in power factor is 20 percent. As we charge at maximally 10% (of kW rating) and the losses in the unit are around 5% of the input current, we will see a nominal input current when charging at a level approximately 5% lower than the maximal nominal output current at load PF 0.8.
 
Resolution:
NA
 
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.