Browse FAQs

Using PowerChute Network Shutdown in a redundant UPS Scenario

Published date: 02 June 2020

Issue:
The purpose of using Power Chute Network Shutdown with a redundant UPS configuration is to confirm that an event is occurring on all UPS before sending a shutdown signal to the connected servers.

Product Line:
Power Chute Network Shutdown

Environment:
All support OS

Cause:
Informational

Solution:

Information concerning configuring PCNS with redundant UPS can be found at this link Application Note #98 


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.