Why is the Protection Working LED of an APC SurgeArrest, or SurgeProtector off?
Published date:
05 June 2020
Issue:
Why is the Protection Working LED of an APC SurgeArrest, or SurgeProtector off?
Product Line:
APC Surge Arrest
Environment:
N/A
Cause:
Reasons the green-colored Working Protection LED of the APC SurgeArrest may not
illuminate:
1. The unit is powered off (for 7 outlet SurgeArrest strips only).
2. The LED is defective.
3. The unit sustained a large power transient and basically died.
4. The unit was heavily overloaded and an internal fuse was tripped.
Resolution:
If one of the items numbered 2 through 4 is the reason, APC will replace the SurgeArrest under its lifetime warranty. First, check that the SurgeArrest unit's circuit breaker is not tripped. Then check that the SurgeArrest unit is plugged into a good, properly functioning power receptacle outlet.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.