InRow Entering Fluid Temp threshold is not alarming
Published date:
03 September 2020
Issue:
InRow Entering Fluid Temp threshold is not alarming
Product line:
InRow
Environment:
Data Center Cooling
Cause:
Resolution:
In the newest firmware ACRC 372 and higher the entering fluid temp alarm threshold violation will not be reported unless two conditions are met. The unit has a >=40% valve position opening, and the entering temperature is above the threshold.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.