Consulter la FAQ

What types of Administrative system level alerts are produced by Data Center Expert?

Date de publication : 27 November 2018

Issue:
Administrative alerts in DCE
 
Product Line:
StruxureWare Data Center Expert
 
Environment:
StruxureWare DCE 7.x
 
Cause:
Administrative alerts are pre-defined in DCE. These alerts will be sent when an event below occurs and email is configured with a local or LADP/AD user account.
 
Resolution:
Here is a list of all the possible notifications a user could receive  from DCE:
  • Cancelled Backup - If a backup is in progress and someone cancels it through DCE User Interface.
  • Critical Communications Error - If a NetBotz appliance drops offline (does not apply to SNMP). - Drive Issues -      (Enterprise server only) - If one of the hard drives in the RAID is bad or rebuilding (the state it will be in after you insert a replacement drive).
  • Email Tests - The test email sent when setting your SMTP (email server) settings.
  • Failed Backup - If a backup starts successfully, but is unable to complete (runs out of disk size, share drops offline, etc...)
  • Failed Schedule Export - Same as "Failed Backup" but for scheduled exports
  • Purging - When the disk is being purged because the usage has reached the limit set in the user interface
  • Reboot - When the server is rebooted.
  • Storage Repository Offline - When DCE uses an external storage repository and it drops offline.
Please note that to be notified for any of these alerts, the user / administrative account must have an e-mail associated with their login either in DCE or, if DCE is configured to use them, in an associated Active Directory / LDAP account.

Cela vous a-t-il aidé ?

Que pouvons-nous faire pour améliorer l'information ?

Vous n'avez pas trouvé ce que vous cherchiez ?

Contactez notre équipe client pour obtenir des informations sur l'assistance technique, l'assistance dédiée aux réclamations et plus encore.