Consulter la FAQ

Why won't my Lithium-Ion Smart-UPS start when the battery is first connected when there is no utility power to the unit?

Date de publication : 23 August 2018


Issue:

When you first connect the battery there is a delay before the unit can start on battery with no utility power present.

Product Line:

Smart-UPS

Environment:

SMTL750RM2UC, SMTL1000RM2UC, SMTL1500RM3UC - All Serial Numbers

Cause:

If the UPS is not connected to AC Power, then there will be up to a 1 minute delay between the initial connection of the battery and the UPS being ready to start.

Resolution:

Wait 1 minute before pressing the ON key, or connect the UPS to AC power to eliminate the delay.
 

Cela vous a-t-il aidé ?

Que pouvons-nous faire pour améliorer l'information ?

Vous n'avez pas trouvé ce que vous cherchiez ?

Contactez notre équipe client pour obtenir des informations sur l'assistance technique, l'assistance dédiée aux réclamations et plus encore.