Consulter la FAQ

What size is the threaded rod of the Ladder Stacking Kit, and will ours fit on other manufacturer's ladder?

Date de publication : 08 April 2019

Issue:
Customers ask for the thread size and dimensions of the threaded rod. They may also ask if the Ladder Stacking Kit can be used on other manufacturer's ladder.

Product Line:
NetShelter SX

Environment:
All versions and serial ranges.

Cause:
Customers need to know the spec of the threaded rod for installation design.

Resolution:
The threaded rod has 5/8"-11 coarse threads. The length is 12".
The Ladder Stacking Kit will mount onto a ladder rail with the maximum dimensions of 1 1/4" tall x 1/2" thick.
NOTE: Although this product is named Ladder Stacking Kit it is used to suspend a ladder. The ladder that's on top must be suspended, probably from above. This kit is then used to suspend another ladder underneath the first one.

Cela vous a-t-il aidé ?

Que pouvons-nous faire pour améliorer l'information ?

Vous n'avez pas trouvé ce que vous cherchiez ?

Contactez notre équipe client pour obtenir des informations sur l'assistance technique, l'assistance dédiée aux réclamations et plus encore.